产品家族

Arc Flash Studies

Arc flash incidents are highly concentrated radiant thermal energy resulting from an arcing fault between two points. These potentially devastating events kill or injure people every day. An up-to-date arc flash study helps mitigate these hazards by calculating the limited and restricted approach boundaries inside which workers must use appropriate personal protective equipment (PPE).

宣传彩页
最适合于:
  • Data CenterColocationHosting
  • Healthcare
  • Manufacturing
  • Oil and Gas
  • Power Generation
  • PowerGas Transmission and Distribution

优点

Improved regulatory compliance results from performing arc flash hazard analysis in accordance with industry guidelines 
Improved worker safety is achieved by identifying potential hazards and implementing recommendations to mitigate risk 
Greater productivity occurs by reducing business disruption and lost man hours that can result from arc flash incidents 
Enhanced system performance results from improved maintenance practices and preventing equipment damage 

特性

Data collection includes critical equipment information that is necessary to perform accurate arc flash hazard analysis
Arc flash calculations are performed with state-of-the-art software and in accordance with the standards of NFPA and IEEE
Comprehensive report, including the results of the hazard analysis and expert recommendations, helps ensure compliance with OSHA and NFPA standards

联系人

支持
显示联系人 California, 91733, USA 更换地点
Electrical Reliability Services
+1 877 468 6384
USA
服务重点领域: 项目服务, 性能优化服务, 应急响应, 预防性的维护, 工业应用预防性维保, 备件及零配件管理
Emergency Response for Services
+1 800 543 2378
USA
服务重点领域: 项目服务, 性能优化服务
Geist Support - Americas (Rack PDU and Watchdog)
+1 888 630 4445
1777 Yolande Avenue Lincoln Nebraska USA
服务重点领域: 项目服务, 性能优化服务, 应急响应, 预防性的维护, 工业应用预防性维保, 远程服务, 备件及零配件管理

常见问题

问题
What is an arcing fault?
回答
An arcing fault is the flow of current through the air between phase conductors or phase conductors and neutral or ground.
问题
What causes an electrical arc?
回答
An arc occurs when electric current flows between two or more separated energized conducting surfaces. Some arcs are caused by human error including dropped tools, accidental contact with electrical systems, and improper work procedures. Another common cause of an arc is insulation failure.
问题
What can happen if I am exposed to arc flash?
回答
Exposure to an arc flash frequently results in a variety of serious injuries, and in some cases, death. Workers have been injured even though they were 10 feet or more away from the arc center.
问题
What can I do to reduce my risk to arc flash exposure?
回答
Preventive maintenance, worker training, and an effective safety program can significantly reduce arc flash exposure.
问题
Are all arcs equal?
回答
No. You must conduct a hazard assessment to determine the level (intensity) of energy from the arc in calories. Then you can determine the proper personal protective equipment (PPE) needed.

选择您的本国语言