Trabalhar com nossa equipe de vendas Vertiv possibilita que designs complexos sejam configurados de acordo com as suas necessidades específicas. Se você pertence a uma organização buscando orientação técnica para um projeto grande, a Vertiv pode proporcionar o suporte de que você necessita.

Saiba mais

Muitos clientes trabalham com um parceiro revendedor da Vertiv para comprar produtos Vertiv para suas aplicações de TI. Os parceiros têm amplo treinamento e experiência, e estão em uma posição única para especificar, vender e dar suporte a todas as soluções de infraestrutura e TI com os produtos da Vertiv.

Encontre um Revendedor

Já sabe do que você precisa? Quer a conveniência da compra on-line e envio? Algumas categorias de produtos Vertiv podem ser adquiridas por meio de um revendedor on-line.


Encontre um revendedor on-line

Precisa de ajuda para escolher um produto? Fale com um Especialista da Vertiv altamente qualificado que o ajudará e orientará para a solução certa.



Entre em contato com um Especialista da Vertiv

University of Pisa relies on Vertiv for data infrastructure capacity expansion to support high-performance computing and AI

27/3/24

Deployed power and liquid cooling solutions respond to the challenges of 'The Hybrid Green Data Centre Expansion' project to improve energy efficiency, reduce operating costs and optimise available space

London, UK [March 27, 2024] - Vertiv, (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, has been selected by the University of Pisa to extend its existing data centre infrastructure and provide the new power and liquid cooling equipment needed to meet the new demands of high-performance computing systems and maintain high operational flexibility. 

The University of Pisa, founded in 1343, is one of the oldest and most prestigious universities in Italy and Europe. Its organisation is made up of 20 departments, which include humanities, sciences and computer sciences, with about 50,000 students enrolled in different degree courses. The University already had three data centres in the city to support teaching and research activities and needed to further enhance the infrastructure to provide greater efficiency and agility. In 2016, the University of Pisa embarked on a project for the development of a new data centre called "The Green Data Centre". Vertiv was chosen to provide the critical power and cooling infrastructure, and the successful implementation of the project led to a strong technical and strategic relationship with the University. More recently, the University turned to Vertiv to expand this data centre and support the infrastructure demands of high-performance computing applications.

“The main objective of our project known as ‘The Hybrid Green Data Centre Expansion’ was to use the available wing of the building, while keeping the original design and user interface intact,” said Maurizio Davini, CTO at the University of Pisa. “We also needed to integrate new technology elements that help to meet the growing demands of high-performance computing, while providing excellent operational flexibility. The requirements have been fully met by Vertiv, which has allowed us to keep energy costs under control for efficient management of our new data centre."

“The increasing adoption of high density and AI applications is demanding innovative infrastructure strategies,” said Giordano (Gio) Albertazzi, CEO at Vertiv. “Vertiv's solutions, including liquid cooling for direct-to-chip applications and high density power systems, will provide the University of Pisa with the capacity they need to support a new generation of computing and future generations of student research." 

Vertiv provided a mix of power, cooling, rack, networking and service solutions, including four Vertiv™ DCC containment solutions for corridor closures. In terms of cooling, the hybrid solution includes twenty Vertiv™ Liebert® CRV row-based cooling units and two Vertiv™ Liebert® PDX-PI direct expansion floor-mount cooling systems with variable speed compressors, as well as three Vertiv™ Liebert® XDU liquid cooling units, which control the temperature and flow of the refrigerant to the servers in a direct-to-chip application. 

Vertiv also supplied several power solutions, including two Vertiv™ Liebert® APM 500 kVA UPS (uninterruptible power supply) systems and VRLA batteries, eight Vertiv™ Liebert® RXA switchgear units, a 400kW Vertiv™ Power Module prefab solution, 76 Vertiv™ Geist™ Switched PDUs (power distribution unit) and 38 Vertiv™ VR racks. In particular, the external Vertiv Power Module enabled the expansion of the data centre despite space constraints within the building. Vertiv provided a turnkey solution, managing the suppliers and subcontractors to complete the interior space with fire detection and extinguishing systems while an external 630kW backup generator was integrated with the Vertiv Power Module. 

Vertiv also provided consulting, design, installation and commissioning services, including the integration of the Vertiv™ Environet™ Alert monitoring software, which allows the customer to remotely monitor the entire infrastructure. 

"Based on the needs highlighted, we suggested to the University of Pisa to adopt Liebert® XDU liquid cooling systems, and then created tailor-made hybrid corridors, which integrate both air cooled and new liquid cooled equipment,” said Andrea Faeti, sales director for enterprise accounts in Italy at Vertiv. “The hydraulic infrastructure has been expanded, allowing previously installed cooling units to supply chilled water to new data centre equipment. In addition, space constraints prompted us to design an external Vertiv Power Module customised to the site's specific requirements. The solution was completed with our monitoring service that provides real-time visibility and control to the entire data centre infrastructure." 

Among the main benefits provided by the newly deployed Vertiv solutions is the implementation of liquid cooling in existing air-cooled data centres. Combining air and liquid cooling is one of the latest trends in thermal management, to enable reduced energy usage for higher capacities of cooling. Finally, the new infrastructure provides a series of benefits such as high resiliency, efficient cooling for high-density equipment, and enhanced monitoring and management to maintain system availability. 

For more information about Vertiv’s work with the University of Pisa, read the case study at this link. To learn more about Vertiv solutions for AI and high-density applications, visit Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) combines hardware, software and services to enable the continuity and operational optimisation of critical infrastructure, supporting its customers' business strategies. Vertiv solves the toughest challenges for data centres, telecommunications networks, and digital facilities for commercial and industrial applications with a comprehensive portfolio of technologies and services for power and continuity, cooling, and IT infrastructure solutions, from the cloud to the edge. Headquartered in Westerville, Ohio (USA) and with a global presence, Vertiv operates in more than 130 countries. For more information, Vertiv news and content updates, please visit Vertiv.com .

About the University of Pisa

The University of Pisa, founded in 1343, is one of the oldest and most prestigious universities in Italy and Europe and the second in Tuscany, after Florence. Its organisation is made up of 20 Departments, which include humanities, sciences and computer sciences, with about 50,000 students enrolled in different degree courses. For more information www.unipi.it 

Forward Looking Statement

This release contains forward-looking statements and forward-looking statements in accordance with the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act and Section 21E of the Securities Exchange Act. These claims are just a prediction. Actual events or results may differ materially from the anticipations and forecasts expressed in this press release. Readers are encouraged to consult Vertiv's filings with the Securities and Exchange Commission, including its most current Annual Report on Form 10-K and any subsequent Quarterly Report on Form 10-Q, for a discussion of these and other important risk factors regarding Vertiv and its business. Vertiv is under no obligation, and expressly disclaims any obligation, to update or change these forward-looking statements, whether as a result of new information, future events, or otherwise. 

Media Contact

Susanna Collins
TEL:  +44 (0)7872 558593
E-mail: susanna.collins@apodpr.co.uk

Faça seu Login Parceiro

Selecione o seu país e idioma