Vertiv 영업담당자에게 문의하시면 고객의 고유한 요구에 맞게 복잡한 설계를 구성할 수 있습니다. Vertiv는 대규모 프로젝트에 대한 기술 지침이 필요한 조직에 필요한 지원을 제공할 수 있습니다.

자세히 보기

많은 고객이 Vertiv 리셀러 파트너와 협력하여 IT 애플리케이션을 위한 Vertiv 제품을 구매합니다. 파트너는 다양한 교육을 받고 전문 경험을 보유하고 있으며 Vertiv 제품을 통해 전체 IT 및 인프라 솔루션을 지정, 판매, 지원할 수 있는 독보적인 위치에 있습니다.

리셀러 찾기

필요한 것이 무엇인지 이미 알고 계십니까? 온라인 구매 및 배송의 편리함을 원하십니까? 특정 범주의 Vertiv 제품은 온라인 리셀러를 통해 구매할 수 있습니다.


온라인 리셀러 찾기

제품 선택에 도움이 필요하십니까? 여러분에게 적합한 솔루션을 안내할 수 있는 우수한 Vertiv 전문가와 상담하십시오.



Vertiv 전문가에게 문의하기

Vertiv Introduces Cell Site Enclosure to Support C-RAN Network Evolution

11월 01, 2017

Flexibility of  Vertiv™ XTE 601E delivers opportunities for reduced costs and equipment footprint

Columbus, Ohio [November 1, 2017]  Vertiv, formerly Emerson Network Power, today introduced the Vertiv XTE 601E, an 84-inch all-in-one outdoor enclosure designed specifically to bring flexibility and a reduced equipment footprint to C-RAN network architectures. Now available to customers in North America, the Vertiv XTE 601E is highly configurable and capable of housing network equipment, DC power and batteries within the same enclosure chamber while tailoring the equipment rack space and a number of battery strings to the needs of the site.
 
That flexibility is critical to C-RAN networks, where electronics traditionally housed at the base of a cell tower can be centralized for use with multiple towers. In turn, this eliminates the need for some enclosures at the cell site, where cellular providers are increasingly seeking options to further reduce equipment footprint and costs.  The Vertiv XTE 601E does just that, allowing providers to house more equipment or more batteries in the enclosure and to adjust that mix as needed. That means the DC power system, battery backup, radio equipment and electronics can be housed in a single, thermally controlled enclosure.
 
C-RAN is a major step forward in cellular network architecture and intelligence, enabling more advanced capacity management, streamlining network operations, and paving the way for 5G,” said Scott Armul, vice president and general manager, DC Power and Outside Plant Products, for Vertiv in the Americas. “Fully leveraging these more intelligent networks requires some fundamental changes to the network infrastructure. The Vertiv XTE 601E delivers the flexibility necessary to make those changes possible and, by reducing the equipment needed to support the network, it helps to reduce capital and operational expenses and service time and costs.”
 
At 84 inches tall, the Vertiv XTE 601E has the capacity to reduce overall cabinet footprint at a site by as much as 75 percent and can support concurrent installation and operation of both macro cell site and C-RAN equipment. That allows cellular providers to make a measured, seamless transition from macro to C-RAN technology.
 
The Vertiv XTE 601E is compatible with either traditional valve-regulated lead acid (VRLA) or nickel-cadmium (NiCad) batteries. Its standard configuration includes two battery boxes, but either or both can be removed and replaced with adjustable rails to accommodate additional equipment. The enclosure is offered with thermal management systems tailored to the environment and the equipment  a heat exchanger in cooler climates or an air conditioner in climates with higher temperatures and/or specific operating needs.
 
For more information on the Vertiv XTE 601E and other communication network solutions from Vertiv, visit www.VertivCo.com.
 
 
About Vertiv
Vertiv designs, builds and services critical infrastructure that enables vital applications for data centers, communication networks and commercial and industrial facilities. Formerly Emerson Network Power, Vertiv supports today’s growing mobile and cloud computing markets with a portfolio of power, thermal and infrastructure management solutions including the ASCO®, Chloride®, Liebert®, NetSure™ and Trellis™ brands. Sales in fiscal 2016 were $4.4 billion. For more information, visit VertivCo.com.
 
Contact
Vince McMorrow
T +614 383 1622
E Vince.McMorrow@Fahlgren.com
PARTNERS
개요
파트너 로그인

언어 & 지역