Vertiv 영업담당자에게 문의하시면 고객의 고유한 요구에 맞게 복잡한 설계를 구성할 수 있습니다. Vertiv는 대규모 프로젝트에 대한 기술 지침이 필요한 조직에 필요한 지원을 제공할 수 있습니다.

자세히 보기

많은 고객이 Vertiv 리셀러 파트너와 협력하여 IT 애플리케이션을 위한 Vertiv 제품을 구매합니다. 파트너는 다양한 교육을 받고 전문 경험을 보유하고 있으며 Vertiv 제품을 통해 전체 IT 및 인프라 솔루션을 지정, 판매, 지원할 수 있는 독보적인 위치에 있습니다.

리셀러 찾기

필요한 것이 무엇인지 이미 알고 계십니까? 온라인 구매 및 배송의 편리함을 원하십니까? 특정 범주의 Vertiv 제품은 온라인 리셀러를 통해 구매할 수 있습니다.


온라인 리셀러 찾기

제품 선택에 도움이 필요하십니까? 여러분에게 적합한 솔루션을 안내할 수 있는 우수한 Vertiv 전문가와 상담하십시오.



Vertiv 전문가에게 문의하기

AI는 액체 냉각을 위한 전환점을 어떻게 만들어내는가

Nigel Gore •

Some data center operators remain skeptical that liquid cooling will make significant inroads into a data center ecosystem dominated by air-cooling systems. It’s hard to fault them for that. They’ve seen multiple projections over the years for how rack densities would climb to levels unsupportable by air cooling, and most of those projections were premature or never realized.

Instead of packing racks with high-density servers to deal with the relentless demand for compute capacity as predicted, operators chose instead to spread out their loads, optimize their air-cooling systems, and increase reliance on cloud computing when that resource became available.

The market simply has not had an appetite for making the changes required to bring liquid to the rack. So, it’s fair to ask, what’s different now?

 

The Link Between Digital Transformation and High-Density Computing

The short answer is the use of high-performance computing (HPC) principles to support applications that a large percentage of businesses are adopting or planning to adopt, most notably artificial intelligence (AI). AI has become integral to digital transformation initiatives for organizations across a range of industries. There’s a good chance your organization is making plans today to leverage the power of AI.

Like current HPC deployments, these business-changing applications require the ability to process massive amounts of data with extremely low latency. But unlike HPC, that data isn’t just in the form of text and numbers. AI applications often process data from heterogenous sources in multiple forms, including large image, audio, and video files. Entering 2020, 73% of AI applications were working with image, video, audio, or sensor data.

Chip manufacturers have responded to the growing demand for multi-format AI applications with more powerful chips. Thermal power densities for leading central processing units (CPUs) and graphics processing units (GPUs) rose sharply in the last two years, after relatively modest growth in the previous five years. Intel’s upcoming Ponte Vecchio GPUs shared by Intel CEO Pat Gelsinger, for example, have thermal power densities that will require liquid cooling.

With more of these high-powered CPUs and GPUs being packed into 1U servers and equipment racks being packed with these 1U servers, we are seeing a growing number of applications with racks densities of 30 kW or higher — and we are still very early in the adoption of AI.

 

Liquid Cooling: The Best — and Only — Alternative

Now it’s the data center industry’s turn to respond. To do that, we have to accept the physical limitations of air cooling — it does not have the thermal transfer capacity required to cool high-density racks, no matter how it is optimized. The best case scenario is that energy costs rise sharply while CPUs and GPUs throttle back their clock speeds to prevent overheating, compromising the performance of the application. The worst case is equipment failure.

In contrast, the liquid cooling technologies available today have the capacity to efficiently and effectively cool racks of 50 kW and higher. It’s been a long time coming, but liquid cooling is finally positioned to penetrate the larger ecosystem the way some predicted it would 15 years ago.

 

Introducing Liquid into Air-Cooled Data Centers

While there are some dedicated liquid cooling facilities being developed, most liquid cooling deployments happening today involve transforming existing air-cooled facilities into hybrid air- and liquid-cooled facilities.

This is by no means a simple transformation. Available liquid cooling technologies, the liquid-to-heat ratio, plumbing runs, the liquid distribution loop, and final heat rejection all require careful planning and engineering.

But the expertise, technologies, and best practices are available today to support a successful and minimally disruptive deployment. And the benefits — beyond supporting the applications businesses will become increasingly dependent on — include packing more capacity in the same footprint, dramatic improvements in efficiency, and lower total cost of ownership.

 

To learn more, download our white paper or contact your local Vertiv representative.

관련 자료

PARTNERS
개요
파트너 로그인

언어 & 지역