Vertiv 영업담당자에게 문의하시면 고객의 고유한 요구에 맞게 복잡한 설계를 구성할 수 있습니다. Vertiv는 대규모 프로젝트에 대한 기술 지침이 필요한 조직에 필요한 지원을 제공할 수 있습니다.

자세히 보기

많은 고객이 Vertiv 리셀러 파트너와 협력하여 IT 애플리케이션을 위한 Vertiv 제품을 구매합니다. 파트너는 다양한 교육을 받고 전문 경험을 보유하고 있으며 Vertiv 제품을 통해 전체 IT 및 인프라 솔루션을 지정, 판매, 지원할 수 있는 독보적인 위치에 있습니다.

리셀러 찾기

필요한 것이 무엇인지 이미 알고 계십니까? 온라인 구매 및 배송의 편리함을 원하십니까? 특정 범주의 Vertiv 제품은 온라인 리셀러를 통해 구매할 수 있습니다.


온라인 리셀러 찾기

제품 선택에 도움이 필요하십니까? 여러분에게 적합한 솔루션을 안내할 수 있는 우수한 Vertiv 전문가와 상담하십시오.



Vertiv 전문가에게 문의하기

How to Achieve Greater Security and Efficiency for In-Band and Out-Of-Band Service Processor Management

You only have to do a quick search on “service processors” to see that tech companies are engaged in an arms race to make their embedded service processors ever more powerful. There’s no question that service processors are making it a lot easier for IT administrators to remotely access, monitor and maintain servers.

Before I became product manager for the Avocent Universal Management Gateway (UMG), I was the Global Data Center Manager for Vertiv. In that position, I learned first-hand about how great modern service processor management tools are. But I also realized these tools introduce risk if not used in a secure and responsible manner. I wanted to leverage service processor power while improving security and performance in our data centers by addressing two key issues:

  • Reducing infrastructure vulnerability. Service processors can introduce risk if not properly managed. For example, they come with universal default passwords and configurations. With so many different service processors, it’s tempting to stick to these defaults which provide hackers with easy entry to the network.

  • Increasing administrative efficiency. As in most large data centers, we manage hundreds of service processors from multiple vendors, each with its own interface and unique configuration. IT administrators must use multiple service processor interfaces, maintain large spreadsheets with the name and IP address of each processor and perform updates server by server. It adds up to a lot of time, resources and money.

The solution to these issues turned out to be right in my own company-the Avocent Universal Management Gateway. The UMG is a converged access and control appliance that is perfectly suited to a mixed service processor environment. Designed for local, remote and out-of-band access, the UMG enables IT administrators to monitor and manage multiple service processors from a single interface.

More Control Yields More Security

Let’s start with how the Avocent UMG can reduce risk. Using the UMG’s built-in LDAP/Active Directory interface, administrators set up authentication and authorization controls just once. They no longer need to create and remember separate credentials for each Service Processor (or get lazy and use the defaults.) Access is easier while compliance with password and user access policies is maintained.

The UMG can also cost efficiently increase the security of providing out-of-band access. With the ability to physically attach up to 40 service processors to a single UMG, IT needs fewer network ports for the out-of-band network. The UMG can reside on a separate, isolated network and function as the central gateway to each service processor. This increases infrastructure security because service processors are no longer directly accessible from the production network.

Unified Management Leads to Greater Efficiency

The Avocent UMG makes life easier for IT staff, starting with automated discovery of each service processor. Using built-in service processor profiles, the UMG automatically discovers new processors, connects to them and populates the new system in its database. Maintenance is simpler too because administrators can use the UMG for bulk updates, such as a vulnerability patch. It automatically disseminates the patch, doing away with the need to make each change server by server.

The appliance can consolidate up to 1024 service processors so that their functions such as console access, power control and sensor monitoring and alerting, can be performed in a centralized and secure fashion

As those late-night gizmo advertisements say, “But wait! There’s more!” that’s true of the Avocent Universal Management Gateway as well. Its capabilities are not limited to service processors. The UMG also integrates digital KVM, serial console, and environmental management so that IT administrators can monitor and manage hundreds or thousands of assets from a single pane of glass. A single UMG can replace multiple legacy management consoles to save a lot of rack space.

Using the UMG as the “brain” in our global data centers as well as several edge locations has proven an excellent choice. Its single point of remote access and control for all of the assets in these locations has minimized the need to physically enter the data centers, increasing security. At the same time, the UMG’s converged view has facilitated consolidated infrastructure management that helps our staff monitor and maintain hundreds of assets more efficiently.

And, if you’re wondering why I am no longer in the data center position, well…one of the reasons is because I liked the UMG and the concept a lot, so I was very excited about the opportunity to manage, promote and further develop it.

The Avocent Universal Management Gateway is a truly unique and innovative solution in the Data Center and IT infrastructure management space.

최신 트렌드, 기술 및 뉴스에 대한 정보를 얻으려면 블로그를 구독하십시오.

관련 자료

PARTNERS
개요
파트너 로그인

언어 & 지역