Vertiv 영업담당자에게 문의하시면 고객의 고유한 요구에 맞게 복잡한 설계를 구성할 수 있습니다. Vertiv는 대규모 프로젝트에 대한 기술 지침이 필요한 조직에 필요한 지원을 제공할 수 있습니다.

자세히 보기

많은 고객이 Vertiv 리셀러 파트너와 협력하여 IT 애플리케이션을 위한 Vertiv 제품을 구매합니다. 파트너는 다양한 교육을 받고 전문 경험을 보유하고 있으며 Vertiv 제품을 통해 전체 IT 및 인프라 솔루션을 지정, 판매, 지원할 수 있는 독보적인 위치에 있습니다.

리셀러 찾기

필요한 것이 무엇인지 이미 알고 계십니까? 온라인 구매 및 배송의 편리함을 원하십니까? 특정 범주의 Vertiv 제품은 온라인 리셀러를 통해 구매할 수 있습니다.


온라인 리셀러 찾기

제품 선택에 도움이 필요하십니까? 여러분에게 적합한 솔루션을 안내할 수 있는 우수한 Vertiv 전문가와 상담하십시오.



Vertiv 전문가에게 문의하기

생각보다 더 간단한(그리고 더 나은) 침수 냉각 데이터 센터의 이해

Brandon Moore •

We All Know Where Data Center Demands Are Heading – Up.

We also know what’s driving the demand: continual changes in rack density (heat and power) to keep pace with high-performance computing trends, including artificial intelligence and machine learning.

But there’s a problem. Traditional technologies like Rear Door Heat Exchanger (RDHx) and Liquid to Chip (LTC) are merely band-aids for legacy air cooling, and can only take heat rejection, power requirements and future flexibility so far.

800x550-zh-cn-news-2021-03-25-1_327235_0.jpg

Intel, NVIDIA, and AMD are producing chips running at 400, and soon to be 500, watts.

 

What’s the Answer? For CGG, It Was Single-Phase Immersion Cooling

In 2010, global geosciences leader CGG dove into single-phase immersion cooling and hasn’t looked back. At the time, its aging 10,000-square-foot legacy data center in Houston, Texas had been mothballed due to obsolescence – suffering from a limited available power envelope and an extremely inefficient Power Usage Effectiveness (PUE) of >2.0. CGG’s goal was to retrofit the data center without any downtime to other systems or their network, minimize capital expenditures by deferring them over time, and limiting ongoing OPEX.

After careful analysis and consideration, CGG selected GRC’s patented immersion cooling solution, ICEraQ®, due to its unique ability to meet all its stated goals. The tailored solution included 4 x 42U racks with a 100 kW cooling capacity (25 kW/rack), all of which was installed within eight weeks of issuing the purchase order.

 

An Inside Look at the Process

800x600-weight-distribution_328838_0.png

800x600-weight-distribution_328838_0.png

800x600-rapid-deployment_328832_0.png

800x600-spatial-simplicity_328839_0.png

800x600-hradware-flexibility_328833_0.png

Simple Day-to-Day Operations

Of course, the adoption of immersion cooling also brought certain changes – but CGG was impressed with those, too. Some changes truly made things easier; others, just different.

800x600-whats-easier_328836_0.png

800x600-whats-different_328837_0.png

The Updated Environment: Calm, Cool and Quiet

After installation, even more benefits became apparent to CGG. Traditional air-cooled data centers often feel like cold, noisy wind tunnels – and require a lot of space. CGG’s upgraded data center is just the opposite. It’s half the size of a comparable kW air-cooled data center. It’s also nearly silent, maintained at a comfortable temperature, well-lit, and organized to view all the ICEraQ systems and CDUs at a glance.

In fact, the whole layout is more ergonomic, technician- and human-friendly overall. Cables are neatly stored in the back of the racks; and racks are spaced for convenient access, not temperature control.

The racks themselves are equally remarkable. Dip your hand in the ElectroSafe coolant, and it feels like a warm bath (and you can, because it’s completely safe.) No matter how hot the equipment runs, the coolant will keep all component temps consistent—within 3 degrees. Mission accomplished.

Hear it Straight From CGG:

“Today there is not really much difference between managing this room and managing another traditional air based computer. Some of the differences as you can see because we’re right in the middle of this room, and it is producing as we speak, there’s no noise, almost no noise, the temperature is very reasonable,
there’s no air draft, there’s none of the things you would normally associate with a very high density computer. So that makes for a much nicer environment overall.”

— Laurent Clerc, VP of Information Technology at CGG

 

Conclusion: It’s Hard to Argue with Silence.

According to CGG, immersion cooling is different, but a better different – simpler, quieter, plus a lot more cost-effective and space-saving than other cooling methods. Best yet, CGG was able to save on both CAPEX and OPEX costs.

PORTALS
개요
파트너 로그인

언어 & 지역