Rivolgiti a un rappresentante di Vertiv che lavorerà al tuo fianco e ti aiuterà a realizzare progetti complessi in base alle tue esigenze. Se la tua organizzazione ha bisogno di assistenza tecnica per un grande progetto, Vertiv può fornirti tutto il supporto necessario.

Ulteriori informazioni

Molti clienti si affidano ai reseller che sono partner di Vertiv per l’acquisto di prodotti ideali per le loro applicazioni IT. Affidati alle elevate competenze dei nostri partner che, grazie ai prodotti Vertiv, sono in grado di offrire soluzioni complete per infrastrutture e applicazioni IT: dalle specifiche alla vendita all’assistenza.

Trova un reseller

Sai già di cosa hai bisogno? Vorresti la comodità dell’acquisto e della spedizione online? Alcune categorie di prodotti Vertiv si possono acquistare tramite un reseller online.


Trova un reseller online

Hai bisogno di aiuto per scegliere un prodotto? Parla con un esperto di Vertiv altamente qualificato che ti orienterà verso la soluzione più adatta.



Contatta un esperto di Vertiv

Is BYOP right for your data center?

11 min. Lettura

Learn a structured framework for evaluating bring your own power (BYOP) for data centers, when dedicated generation can improve the development path, and when other options may present less risk.

Download the white paper

In many markets, grid capacity and interconnection timelines are struggling to keep pace with data center demand. Grid-connection waits can extend beyond a decade in some U.S. markets, while utilities are introducing new operating requirements for very large loads.

These pressures are increasing interest in BYOP, dedicated onsite or adjacent generation serving some or all a data center’s normal electrical load. BYOP can improve time to power and reduce dependence on constrained utility capacity.

But BYOP is not necessarily a shortcut around grid constraints. Fuel availability, permitting, emissions, land and water requirements, interconnection, equipment lead times, operations, and long-term economics can create new constraints.

This white paper provides a structured framework for determining whether BYOP improves the development path for a specific project.

The status quo

BYOP should be evaluated as one option within a broader power strategy, not assumed to be the answer whenever utility capacity is constrained.

The framework begins with an assessment of utility service, including capacity, timing, required upgrades, study requirements, costs, and operating conditions. Developers then compare alternatives such as phased development, relocation, expansion of an existing site, cloud or colocation capacity, co-location with existing generation, and BYOP.

The key question is whether BYOP improves the project’s overall risk profile compared with those alternatives.

Inside the framework

If BYOP remains viable, the framework helps developers define its intended use before selecting technology, separate ownership, site, and commercial decisions, assess site and permitting feasibility, and compare likely technology and fuel options.

A bridge to utility service, grid-connected supplemental system, or long-term islanded approach creates different requirements for how generation interacts with utility service and how the project evolves. Ownership, physical connection, and commercial structure are also treated as separate decisions.

Site feasibility is evaluated against constraints such as land, fuel, permitting, emissions, water, utility requirements, safety, and community acceptance. Technology and fuel options are compared against deployment time, cost, reliability, maintainability, load-following capability, emissions, cooling requirements, scalability, and grid interaction.

The framework is structured but iterative. Findings may require developers to revisit earlier assumptions or reconsider whether BYOP remains justified.

The bottom line

BYOP should move forward when dedicated generation improves the project’s overall risk profile compared with the available alternatives. Any schedule or capacity advantage must be weighed against added fuel, permitting, land, emissions, interconnection, capital, operating, and long-term asset risks.

Download the white paper to learn how to evaluate whether BYOP should be part of your data center infrastructure development strategy.

+

AI Intelligenza artificiale Critical power Critical Power Innovazione nei data center Efficienza Emergency Services Autonomia energetica Densificazione estrema Ottimizzazione della struttura Campus su scala gigawatt Trasformazione dell’architettura di alimentazione TCO - Costo totale di proprietà
Login dei partner

Lingua & Ubicazione