Rivolgiti a un rappresentante di Vertiv che lavorerà al tuo fianco e ti aiuterà a realizzare progetti complessi in base alle tue esigenze. Se la tua organizzazione ha bisogno di assistenza tecnica per un grande progetto, Vertiv può fornirti tutto il supporto necessario.

Ulteriori informazioni

Molti clienti si affidano ai reseller che sono partner di Vertiv per l’acquisto di prodotti ideali per le loro applicazioni IT. Affidati alle elevate competenze dei nostri partner che, grazie ai prodotti Vertiv, sono in grado di offrire soluzioni complete per infrastrutture e applicazioni IT: dalle specifiche alla vendita all’assistenza.

Trova un reseller

Sai già di cosa hai bisogno? Vorresti la comodità dell’acquisto e della spedizione online? Alcune categorie di prodotti Vertiv si possono acquistare tramite un reseller online.


Trova un reseller online

Hai bisogno di aiuto per scegliere un prodotto? Parla con un esperto di Vertiv altamente qualificato che ti orienterà verso la soluzione più adatta.



Contatta un esperto di Vertiv

Four dimensions of efficiency: A systems approach to digital infrastructure design

4 min. Lettura

Efficiency in digital infrastructure now spans four critical dimensions: energy, water, materials, and carbon. Learn how integrated system design helps data center operators balance performance with long-term resource management, environmental responsibility, and cost considerations.

As digital infrastructure expands to respond to increasing demand, efficiency has evolved beyond a single-metric conversation. Today's data center operators face growing demands on energy systems, water resources, materials, and physical equipment—all while managing rising rack densities and compressed deployment timelines.

The reality is that infrastructure decisions made today about power architecture, thermal systems, equipment selection, and deployment strategy create operational and resource implications that may persist for decades of service life. Beyond isolated roles that cascade through project phases, data center operators need to answer crucial questions: how much energy a facility consumes, how effectively it uses water, how much material waste it generates, and its carbon footprint from manufacturing through decommissioning.

Efficiency across the full system has become increasingly important to managing reliability, scalability, and total cost of ownership. At Vertiv, we address these challenges through a systems-based approach to digital infrastructure design, embedding responsible business principles directly into how products and systems are engineered, deployed, and supported across their lifecycle.

Beyond component optimization: Four key efficiency dimensions

Rather than optimizing individual components in isolation, effective infrastructure design integrates four efficiency dimensions that have become baseline expectations for modern deployments:

  1. Energy efficiency: System-level energy performance depends on how components work together under real operating conditions. System-level efficiency strengthens resilience and long-term operating discipline. Integrated design choices—from power distribution architecture to thermal management strategies—enable operators to reduce energy consumption while maintaining performance and reliability. All the while supporting customers’ goals and performance objectives. Beyond meeting Greenergy and Polar's technical requirements and specifications, Vertiv designed integrated power and thermal architectures that support electrical efficiency and high-density workloads.
  2. Water stewardship: Where practical, reducing water demand supports operational resilience and addresses resource constraints. Design strategies may include optimizing cooling system selection for local climate conditions, implementing water-side economization where feasible, or specifying systems that require minimal water consumption. Depending on climate and configuration, cooling solutions may improve power usage effectiveness (PUE) and water usage effectiveness (WUE) through economization, hybrid wet-dry operation, and water-efficient operating modes—helping operators like Inwi and Colt Technology Services reduce operational costs while managing resource consumption across their infrastructure portfolios.
  3. Material resource management: Lifecycle thinking begins at the design stage. Considerations include design for serviceability, component longevity, modularity to enable phased capacity growth, and end-of-life planning. These choices can help limit material waste while supporting operational flexibility and long-term asset value. Integrated and prefabricated systems can reduce construction complexity, shorten deployment timelines, and limit on-site material waste. For Greenergy and Polar, this modular approach enables phased capacity expansion to match evolving workload demands without requiring full-system replacement.
  4. Carbon management: Managing carbon impacts requires attention across the full lifecycle—from manufacturing and transportation to in-use energy consumption and eventual decommissioning. While operational energy typically represents the largest share of lifecycle carbon, system design decisions influence emissions at every stage. Integrated design choices drive carbon efficiency across the infrastructure lifecycle: energy-efficient power and cooling systems, grid-responsive integration, low-GWP refrigerant transitions, and modular construction methods. These system-level decisions help Polar and other customers in other regions manage carbon impacts while supporting demanding workload requirements.

Integrated design in practice

These four dimensions are not managed as parallel efforts. They are embedded in Vertiv's product and system design, prioritizing initiatives that strengthen operational discipline and facilitate reliable performance in real-world conditions.

This deliberately pragmatic approach recognizes that customers need infrastructure solutions that balance performance with long-term cost and resource considerations. It means:

  • Designing for system-level outcomes, not isolated component metrics
  • Supporting operational discipline through reliable, serviceable equipment
  • Enabling informed decisions with transparent lifecycle data
  • Adapting to site-specific conditions rather than one-size-fits-all solutions
  • Actual performance varies by site conditions and operating profiles, which is why the Vertiv approach emphasizes flexibility, field-proven reliability, and lifecycle support.

Responsible business as operational practice

Efficiency is not an add-on feature—it's intrinsic in how we execute strategy every day. From initial specification through deployment and ongoing operation, Vertiv applies responsible business principles to help customers achieve their operational and resource management objectives.

This is "One Vertiv, One World" in practice: designing efficient products and systems that manage accountability across the lifecycle of infrastructure, supporting customers as they scale digital infrastructure responsibly.

Learn more about how Vertiv integrates efficiency, reliability, and accountability into product and system design. Read the latest Vertiv 2025 Responsible Business Report to see how responsible business principles are embedded in real-world infrastructure solutions.


Blogpost AI Intelligenza artificiale Conformità e sicurezza Critical power Innovazione nei data center Design incentrato sul digitale Autonomia energetica ESG/sustainability Trasformazione dell’architettura di alimentazione Thermal Management

VertivTM AI Hub

Un'infrastruttura progettata per supportare con anticipo più generazioni di piattaforme di calcolo, a partire da ORA.

Ulteriori informazioni
Login dei partner

Lingua & Ubicazione