Rivolgiti a un rappresentante di Vertiv che lavorerà al tuo fianco e ti aiuterà a realizzare progetti complessi in base alle tue esigenze. Se la tua organizzazione ha bisogno di assistenza tecnica per un grande progetto, Vertiv può fornirti tutto il supporto necessario.

Ulteriori informazioni

Molti clienti si affidano ai reseller che sono partner di Vertiv per l’acquisto di prodotti ideali per le loro applicazioni IT. Affidati alle elevate competenze dei nostri partner che, grazie ai prodotti Vertiv, sono in grado di offrire soluzioni complete per infrastrutture e applicazioni IT: dalle specifiche alla vendita all’assistenza.

Trova un reseller

Sai già di cosa hai bisogno? Vorresti la comodità dell’acquisto e della spedizione online? Alcune categorie di prodotti Vertiv si possono acquistare tramite un reseller online.


Trova un reseller online

Hai bisogno di aiuto per scegliere un prodotto? Parla con un esperto di Vertiv altamente qualificato che ti orienterà verso la soluzione più adatta.



Contatta un esperto di Vertiv

Important Considerations When Implementing DCIM

Implementations in the data center are usually about technology—a new device providing greater power, speed, flexibility and so forth. It’s not to say that DCIM isn’t a technology, but it’s important to realize that DCIM isn’t just a technology implementation—it’s a business solution for your data center. This means it should be implemented in the same way a new business solution is introduced. Here are some considerations to keep in mind:

  • Think big, but start small.​
    Define the strategic, long-term goals for your DCIM initiatives. Then, rather than going for the big bang, identify the most pressing issues related to the overall strategy and implement the DCIM capabilities in phases to reap value incrementally. Learn more about determining which DCIM functions are essential.
  • Create a strong partnership.​
    Modern business application development uses an agile, iterative approach with business and IT working as partners. Because DCIM can transform your IT and Facilities operations, collaboration between these groups is essential. As part of the transformation, people will do their jobs in new ways, so it is important to help them understand how these changes will benefit them, allow them to participate in the transformation process and train them to succeed.
  • Capacity Planning and Management.​
    With the ability to accurately plan power and cooling requirements, what are the savings in delayed equipment purchases and/or building a new data center? In addition, with tools that make capacity planning easier and faster, how much time per day is your staff saving on this task?
  • Implementation is just the beginning of the journey.​
    Because change is on-going, DCIM reflects the fluid nature of the data center, providing the flexibility and agility needed to support changing requirements. As you implement DCIM in your organization, revisit your plan regularly, adjusting it to suit changing needs and priorities.

Articoli correlati

Selling DCIM Internally Image

Argomenti degli articoli

Selling DCIM Internally
Return on Investment Image

Argomenti degli articoli

Return on Investment
Essential DCIM Functions Image

Argomenti degli articoli

Essential DCIM Functions
Evaluating the Promise of DCIM Image

Argomenti degli articoli

Evaluating the Promise of DCIM
Login dei partner

Lingua & Ubicazione