Al trabajar con el soporte de ventas de Vertiv, puede configurar los complejos diseños de acuerdo con sus necesidades específicas. Si forma parte de una organización que busca orientación técnica para un proyecto grande, Vertiv puede ofrecerle el soporte que necesita.

Más información

Muchos clientes trabajan con un socio revendedor de Vertiv para comprar productos de Vertiv para sus aplicaciones de TI. Los socios cuentan con amplia capacitación y experiencia, y están en una posición única para especificar, vender y brindar soporte a soluciones completas de TI e infraestructura con los productos de Vertiv.

Buscar un revendedor

¿Ya sabe lo que necesita? ¿Desea la comodidad de comprar y enviar en línea? Ciertas categorías de productos de Vertiv se pueden comprar a través de un revendedor en línea.


Encontrar un vendedor en línea

¿Necesita ayuda para elegir un producto? Hable con un especialista de Vertiv altamente calificado, quien le guiará hacia la solución adecuada para usted.



Contactar a un especialista de Vertiv

Is BYOP right for your data center?

12 min. Leer

Learn a structured framework for evaluating bring your own power (BYOP) for data centers, when dedicated generation can improve the development path, and when other options may present less risk.

Download the white paper

In many markets, grid capacity and interconnection timelines are struggling to keep pace with data center demand. Grid-connection waits can extend beyond a decade in some U.S. markets, while utilities are introducing new operating requirements for very large loads.

These pressures are increasing interest in BYOP, dedicated onsite or adjacent generation serving some or all a data center’s normal electrical load. BYOP can improve time to power and reduce dependence on constrained utility capacity.

But BYOP is not necessarily a shortcut around grid constraints. Fuel availability, permitting, emissions, land and water requirements, interconnection, equipment lead times, operations, and long-term economics can create new constraints.

This white paper provides a structured framework for determining whether BYOP improves the development path for a specific project.

The status quo

BYOP should be evaluated as one option within a broader power strategy, not assumed to be the answer whenever utility capacity is constrained.

The framework begins with an assessment of utility service, including capacity, timing, required upgrades, study requirements, costs, and operating conditions. Developers then compare alternatives such as phased development, relocation, expansion of an existing site, cloud or colocation capacity, co-location with existing generation, and BYOP.

The key question is whether BYOP improves the project’s overall risk profile compared with those alternatives.

Inside the framework

If BYOP remains viable, the framework helps developers define its intended use before selecting technology, separate ownership, site, and commercial decisions, assess site and permitting feasibility, and compare likely technology and fuel options.

A bridge to utility service, grid-connected supplemental system, or long-term islanded approach creates different requirements for how generation interacts with utility service and how the project evolves. Ownership, physical connection, and commercial structure are also treated as separate decisions.

Site feasibility is evaluated against constraints such as land, fuel, permitting, emissions, water, utility requirements, safety, and community acceptance. Technology and fuel options are compared against deployment time, cost, reliability, maintainability, load-following capability, emissions, cooling requirements, scalability, and grid interaction.

The framework is structured but iterative. Findings may require developers to revisit earlier assumptions or reconsider whether BYOP remains justified.

The bottom line

BYOP should move forward when dedicated generation improves the project’s overall risk profile compared with the available alternatives. Any schedule or capacity advantage must be weighed against added fuel, permitting, land, emissions, interconnection, capital, operating, and long-term asset risks.

Download the white paper to learn how to evaluate whether BYOP should be part of your data center infrastructure development strategy.

+

AI Inteligencia artificial Potencia Crítica Critical Power Innovación del centro de datos Eficiencia Emergency Services Autonomía de la energía Densificación extrema Optimización de instalaciones Campus a escala de gigavatios Transformación de la arquitectura de alimentación Costo total de propiedad
Iniciar Sesion Como Socio

Idioma y ubicación