Al trabajar con el soporte de ventas de Vertiv, puede configurar los complejos diseños de acuerdo con sus necesidades específicas. Si forma parte de una organización que busca orientación técnica para un proyecto grande, Vertiv puede ofrecerle el soporte que necesita.

Más información

Muchos clientes trabajan con un socio revendedor de Vertiv para comprar productos de Vertiv para sus aplicaciones de TI. Los socios cuentan con amplia capacitación y experiencia, y están en una posición única para especificar, vender y brindar soporte a soluciones completas de TI e infraestructura con los productos de Vertiv.

Buscar un revendedor

¿Ya sabe lo que necesita? ¿Desea la comodidad de comprar y enviar en línea? Ciertas categorías de productos de Vertiv se pueden comprar a través de un revendedor en línea.


Encontrar un vendedor en línea

¿Necesita ayuda para elegir un producto? Hable con un especialista de Vertiv altamente calificado, quien le guiará hacia la solución adecuada para usted.



Contactar a un especialista de Vertiv

BYOP for data centers: Why implementation planning determines success

4 min. Leer

Choosing BYOP is only the beginning. Successful implementation requires generation, data center infrastructure, utility requirements, controls, and operations to be planned as an integrated system.

Power constraints, lengthy grid connection timelines, and rapidly growing data center and AI power demand are leading more owners and developers to consider "bring your own power" (BYOP) to improve time to power and reduce dependence on constrained utility capacity. But selecting BYOP is only the beginning. Once that decision is made, how the project is planned, designed, integrated, validated, and operated strongly influences whether it preserves its intended time-to-power advantage.

“Bring your own power (BYOP) for data centers: Five critical success factors for implementation,” addresses the next stage of the BYOP journey. Rather than revisiting whether BYOP is the right strategy for a project, it focuses on five implementation priorities: early coordination with utilities, authorities, and partners; co-design of generation and data center infrastructure; early modeling and design validation; standardized and prefabricated solutions where appropriate; and a clearly defined operating model.

Why BYOP requires integrated planning and execution

BYOP changes the operating architecture of a data center by making prime power generation part of the system that normally supports the critical IT load. This adds or expands responsibilities for fuel supply, utility coordination, emissions compliance, controls integration, and operation of the generation plant. Treating generation, electrical infrastructure, cooling, controls, and IT load as separate workstreams can increase the risk of late-stage redesign, approval delays, control conflicts, and commissioning problems.

One of the more technically significant sections addresses how AI training workloads interact with on-site generation. These workloads can introduce rapid and repeated power changes that onsite generators may not be designed to follow directly. A large interconnected utility grid can better absorb load changes across broader generation, aggregate inertia voltage support, and balancing resources. An onsite or adjacent generation plant has more limited response capability and may therefore be more directly affected by rapid changes in the data center's load.

If those interactions are not adequately addressed, potential system-level risks include unstable operation during fast load changes, reduced efficiency, nuisance trips, control conflicts among generation, uninterruptible power supply (UPS), battery energy storage systems (BESS), and other systems, and limits on how much generation capacity can be used reliably.

Why modeling and validation need to start early

Large grid-connected BYOP projects may be subject to utility or transmission-operator requirements for detailed system modeling and analysis. Depending on the project, required studies may include dynamic and electromagnetic transient (EMT) models, protection studies, fault ride through (FRT) analysis, harmonic studies, and equipment and controls models, with tools such as PSCAD used for EMT simulation.

Modeling and validation planning must begin early, with defined responsibilities, source data, model formats, submission dates, acceptance criteria, and a clear approach to handling proprietary vendor information. As the design evolves, models should remain aligned with equipment selections, firmware, control logic, protection settings, and intended operating modes. As-built models should reflect the final system and, where practical, be correlated with factory and commissioning test results.

Digital twin tools are positioned as integration risk-management instruments, useful for exposing conflicts among physical layout, electrical architecture, cooling systems, control logic, and expansion strategy before they lead to commissioning failures.

Standardization as a schedule discipline

The time-to-power benefit of BYOP can be undermined if every project requires a fully bespoke design. Once the integrated architecture is defined, project teams should standardize the parts of the design that are repeatable and focus custom engineering on site-specific requirements that materially affect performance, permitting, or reliability.

Repeatable reference designs, standardized interfaces, and factory-integrated prefabricated solutions can reduce unnecessary variation, engineering effort, procurement complexity, and installation and commissioning risk. Interfaces that may lend themselves to standardization include medium-voltage distribution, protection schemes, UPS and BESS integration, cooling modules, controls interfaces, and commissioning procedures.

Standardized capacity blocks can also make phased expansion easier as IT load and available power increase.

The operating model gap

Perhaps the most overlooked dimension: many data center operators lack the capabilities required to run a prime power plant. BYOP introduces dispatch authority, fuel procurement, maintenance scheduling, outage coordination, emissions compliance, cybersecurity obligations, and emergency response procedures that fall outside the scope of traditional data center operations.

These responsibilities should be assigned before design and contracting are finalized. For third-party or independent power producer models, contracts must define capacity commitments, maintenance windows, outage notification protocols, data access rights, expansion provisions, and remedies for missed service levels.

The bottom line

BYOP can improve time to power, but preserving that advantage requires coordinated planning across generation, data center infrastructure, controls, the utility interface, and operations. Projects that treat onsite generation as a separate upstream asset increase the risk of integration problems, stranded capacity, commissioning delays, operational gaps, and loss of the intended time-to-power advantage.

For data center teams moving from BYOP strategy to implementation, the white paper provides practical guidance organized around five critical success factors.


AI Inteligencia artificial Disponibilidad y funcionamiento Potencia Crítica Innovación del centro de datos Diseño centrado en lo digital Autonomía de la energía Densificación extrema Optimización de instalaciones Field Evaluation Campus a escala de gigavatios Transformación de la arquitectura de alimentación Infraestructura unificada

Centro de IA VertivTM

Infraestructura diseñada para ir por delante de varias generaciones de computación, a partir de ahora.

Más información
Iniciar Sesion Como Socio

Idioma y ubicación