Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Battery precision is the foundation of AI power stability

12 min. Read

As GPU clusters ramp up and down in milliseconds, the gap between stable operations and costly infrastructure failure comes down to one thing: how accurately your battery system knows its own state.

Download the white paper

Artificial intelligence (AI) infrastructure runs fast. Power management for AI needs to be precise, stable, and reliable.

Modern AI workloads — from large language model (LLM) training to real-time inference — generate rapid, large-burst power patterns that cycle between idle and peak draw in fractions of a second. These fluctuations propagate upstream and stress generators, transformers, switchgear, and utility connections.

For years, operators have worked around this challenge with familiar but imperfect tools: oversizing upstream infrastructure to absorb worst-case spikes, imposing software-based power caps on graphics processing unit (GPU) clusters to artificially limit peak draw, or managing generator instability reactively through operations teams. These approaches reduce exposure but don’t eliminate it. They also come at a cost: higher capital expenditure (CapEx), reduced compute utilization, and longer job completion times.

Input power smoothing (IPS): Manage and prevent consequences

Input power smoothing (IPS) uses integrated lithium battery cabinets working in tight coordination with Vertiv™ power converters to act as an active energy buffer between AI loads and upstream power sources. When load fluctuations stay within UPS capacity, the battery stays out of the loop entirely. Upstream sources see a stable, controlled demand profile. When load spikes exceed capacity, the battery steps in as a short-duration energy source, absorbing the volatility before it reaches the grid.

State of charge (SOC) and state of health (SOH) accuracy

IPS is only as reliable as the data driving these collective patterns and insights.

At the heart of every IPS decision is the battery management system (BMS). Specifically, two metrics calculating millions of data points with precision: State of charge (SOC) and state of health (SOH). When SOC and SOH are communicated accurately, the uninterruptible power supply (UPS) can make real-time decisions to balance IPS performance with backup protection.

In this research, discover:

  • Why AI load volatility increases dependence on accurate battery state reporting
  • What accurate and precise reporting enables across near-, medium-, and long-term operations
  • How engineered integration between the battery cabinet and UPS makes IPS effective for modern AI load profiles

Accurate SOC protects uptime. Accurate SOH protects the lifecycle. Engineered integration makes it work.

Download the white paper to understand why precision battery management is a strategic advantage for AI infrastructure at scale.

+

AI Artificial intelligence Availability & uptime Data center innovation Efficiency Power architecture transformation Total Cost of Ownership

VertivTM AI Hub

Infrastructure designed to stay multiple compute generations ahead, starting now.

Learn more
Partner Login

Language & Location