Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Vertiv Launches New Line of Rackmount UPS to Support the Largest Network Edge Applications

June 17, 2020

Vertiv™ Liebert® GXT5 offers models up to 10 kVA

Miami, FL. [June 17, 2020] – Vertiv (NYSE: VRT), a global supplier of continuity and critical digital infrastructure solutions, today announced the addition of new models of the Vertiv™ Liebert® GXT5 family of rackmount, on-line uninterruptible power supply (UPS) systems. These new models, with capacities of between 500 VA And 10 kVA, are available in 120 V and 208 V configurations from Vertiv wholesalers in Colombia, Costa Rica, Ecuador, El Salvador, Guatemala, Panama, Dominican Republic and the Caribbean.

The Liebert GXT5 has a power factor of up to 1.0 and is more efficient than previous models in both on-line mode (up to 95 percent) and Active ECO™ mode (up to 98 percent). All Liebert GXT5 models are ENERGY STAR 2.0 certified and are compliant with RoHS and REACH.

“Now more than ever, protecting critical infrastructure is vital for companies. Liebert GXT5 UPS units are a solution to protect critical network edge infrastructure and small IT environments, which require low latency and high availability to offer advanced applications and services,” said Ricardo Duque, Vice-President of Channel Strategies for Latin America at Vertiv.

The Liebert GXT5 offers scalable runtime options, with additional external battery cabinets that ensure availability even during extended interruptions. It can be managed remotely and has integrated maintenance bypass and flexible output receptacle configurations to meet the connected equipment requirements of any site. When used together with the free Trellis™ Power Insight software from Vertiv, users can monitor and manage up to 100 supported Vertiv devices.

Along with the highest level of equipment protection available in a rack/tower configuration, the Liebert® GXT5 offers a two-year full coverage factory warranty for the UPS. Vertiv also offers service packages to support individual customer needs.

For more information on the Liebert GXT5 UPS, Vertiv and the Vertiv Channel Partner Program, visit Vertiv.com or social media: Facebook, LinkedIn, and Twitter.

 

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to ensure its customers’ vital applications run continuously, perform optimally and grow with their business needs. As Architects of Continuity™, Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 20,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

 

CONTACT
Ivis Fernandez
P +3053355883
E ivis@fusioncomminc.com

Partner Login

Language & Location