Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Two Key Elements in the Transformation of Data Centers in Latin America: Integration of Artificial Intelligence and Energy Efficiency

The evolution of data centers is in full swing, driven by the growing demand for data and the rapid advance of artificial intelligence. With these technologies, there will be a greater need for high-density power and cooling, along with innovations for more environmentally efficient solutions:

  • Integration of Artificial Intelligence

In response to  the increased adoption of AI and high performance compute (HPC),  the sector is preparing to deploy the necessary infrastructure to meet the required power and cooling capacity. This advancement entails an increase in high-density power and cooling needs, along with innovations for more energy efficient solutions.

The implementation of AI in the data center allows:

 

  • Anomaly detection: It can identify unusual patterns and detect issues before they begin. This real-time detection mitigates potential risks before damages occur.
  • More proactive security measures: AI enables data centers to predict potential threats and vulnerabilities.
  • Data protection: Data centers can enhance data processing, storage, and security. This helps protect uptime, reliability, and integrity of critical business data, both in transit and stored.
  • Pursuit of Energy Efficiency

Sustainability has become a cornerstone in the planning and operation of data centers. Vertiv is committed to innovating technologies to support energy efficient strategies for AI and HPC loads. Liquid cooling technology for racks, in addition to air cooled systems for the data center, is an energy-efficient hybrid solution.

Vertiv also supports the use of alternative energy, smart grids, hybrid networks, battery energy storage systems (BESS). These innovative data center designs offer reliable solutions for customers, reduce carbon production, and reduce impact and dependence on the electrical grid.

This article was a collaboration between Vertiv and Ingenium. Ingenium has over 15 years of experience as a partner in the journey towards decarbonization through the adoption of high-impact environmental practices and can guide you through the process of obtaining certifications such as CEEDA, LEED, and EDGE, among others.

Ingenium, in partnership with Vertiv, aims to complement their technologies and expertise to offer comprehensive solutions that support current technologies in terms of sustainability and energy efficiency in data centers in the region.

PARTNERS
Partner Login

Language & Location