Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Vertiv Ranked as Global Leader in Rapidly Evolving Data Center Cooling Market

December 02, 2020

Research by Omdia reveals that sustainable and innovative technologies such as chilled water and evaporative cooling, as well as forms of liquid cooling, are becoming more widely adopted

Mumbai, India [December 2, 2020] Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, has been ranked by technology analyst firm Omdia as the largest global supplier in a data center cooling market which continues to undergo change and innovation. The newly released research highlights that established heat rejection technologies such as Direct Expansion (DX), Chilled Water and Evaporative Cooling continue to dominate while also becoming more sustainable. In addition, new technologies, such as forms of liquid cooling, are predicted to grow as data center operators look for ways to further improve efficiency and deal with increasingly power-intensive compute.

The Omdia paper, Data Center Thermal Management Report 2020, published in late 2020 and based on 2018 and 2019 data, states that Vertiv has a 23.5% share of the global data center cooling market – more than 10% higher than its nearest rival. The market for data center thermal technology is set to increase from $3.3bn in 2020 to more than $4.3bn in 2024, according to Omdia. Vertiv also leads the global market for perimeter thermal technologies with a 37.5% market share which is more than 20% higher than the next largest supplier.

In addition to analysing market position, the report provides insight and intelligence on how data center cooling technology is evolving. Established technologies such as chillers and perimeter cooling will remain a large proportion of the market. According to Omdia, split DX is still the primary form of heat rejection in data center thermal management, but chilled water and direct evaporative heat rejection are gaining momentum. In addition, cloud and colocation service provider momentum has accelerated, driving double-digit growth for air handling units (AHU).

Omdia predicts there will also be strong growth in forms of liquid cooling – immersion and direct-to-chip – that are expected to double between 2020 and 2024. Several factors are contributing to this shift, including increasing chip and server power consumption, edge growth, increasing rack densities, as well as energy efficiency and sustainability requirements.

Lucas Beran, principal analyst for Omdia’s cloud and data center research practice and the report’s author, said: “The data center thermal management market is on the cusp of an inflection point. Currently, existing air-based thermal products and solutions are driving growth but are limited by their ability to cool 10kW+ rack densities. New technologies, products, and designs are coming to market to help support these high-density deployments and more efficient operations leading to changing market dynamic through 2024.”  

“With the rise in demand for heat rejection technologies, growth in edge computing, and increasing rack densities, data centers are increasingly looking for sustainable and energy efficient liquid cooling solutions - immersion and direct-to-chip. Being ranked as one of the leaders in the rapidly evolving cooling market is a testament to Vertiv’s commitment to constantly innovating our digital infrastructure solutions to support these continuously evolving requirements of our customers,” said Raghuveer Singh, director, thermal management for Vertiv in India. 

In addition to internal innovations, Vertiv is also working with industry thought leadership groups and recently became a Platinum Member of the Open Compute Project (OCP). Vertiv’s role will include supporting initiatives on the adoption of liquid cooling through the Advanced Cooling Solutions (ACS) and Advanced Cooling Facility (ACF) projects. The aim is to bring guidelines and best practices for direct-to-chip and immersion liquid cooling technologies as well as enable practices for data center facilities to adopt liquid cooling.

Vertiv’s own research into thermal technologies also points to future innovation. According to Vertiv’s Data Center 2025: Closer to the Edge report, the data center industry has seen a large-scale shift to economization driven by hyperscale operators and colocation providers, while simultaneously driving heat removal closer to servers through rear door and liquid cooling systems designed to support the high-density racks common in high performance computing (HPC) facilities. Of the 800+ data center professionals that responded to the survey, 42% expect future cooling requirements to be met by mechanical systems, while 22% say they will be met with liquid cooling and outside air, a result likely driven by the more extreme rack densities being observed today.

To learn more about how Vertiv can help data center owners and operators to scale with confidence, visit https://www.vertiv.com/en-in/campaigns/scale-with-confidence/ 

 

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to ensure its customers’ vital applications run continuously, perform optimally and grow with their business needs. As Architects of Continuity™, Vertiv solves the most important challenges facing today’s data centres, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 20,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

 

CONTACT

Ipshita Balu

+91 95901 11798

ipshita.balu@archetype.co

PRODUCTS & SERVICES
Overview
PARTNERS
Overview
Consultants Corner
Partner Login

Language & Location