Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Advantages and Efficient Use of Programmable Sockets

January 01, 2017

UPS in the 0-3 kVA range are connected to the load and mains through sockets, which are normally type IEC320. In several markets, they are replaced by connectors adapted to the local needs (Schuko, NEMA, etc.), however, IEC320 C13 or C14 are more frequently used because of their international scope.

Pluggable UPS have a distinctive feature in the use of these sockets versus hardwired UPS. In the most recent generation of new products, these pluggable UPS include programmable sockets (also referred to in technical literature as “load segments”, “programmable receptacles”, “controlled outlets”, etc.). These sockets can be enabled/disabled separately so that the loads connected to them are powered on/off depending on various conditions.

This feature of programmable sockets provides an extra level of control and protection over the secure energy supplied to the load. In addition, there is an extra value in terms of efficiency and energy optimization (especially when used in combination with Advanced ECO mode).

This paper provides some information about the technical points to be taken into consideration (since not every UPS product in the market has the same performance), as well as several application examples about this powerful feature.

Related Articles

PARTNERS
Overview
Consultants Corner
Partner Login

Language & Location