Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

By combining air and liquid cooling technologies into the next generation of
high-density cooling solutions

 

Do I really need liquid cooling?

Why liquid cooling?

liquidcooling-1.png

Liquid cooling can effectively manage up to and exceeding 120kw per rack

Learn more
liquidcooling-2.png

Reduce total data center power consumption around 10.2%

Learn more
liquidcooling-3.png

More than 15 percent improvement in total
usage effectiveness (TUE)

Learn more
 

What to consider before deploying liquid cooling

Here is high-level guidance any team can use to navigate the incremental addition of liquid cooling to air-cooled environments cooling infrastructure.

Vertiv solutions and services

 

Choose your path to high-density

Your journey to high-density can be a smooth ride. No matter its starting point or final destination

Vertiv is working together with leaders in the AI industry

Adding Vertiv expertise to the NVIDIA Partner Network

Vertiv and NVIDIA collaborated to develop a unique AI cooling solution for the COOLERCHIPS program and formalized our partnership when Vertiv joined the NVIDIA Partner Network. NVIDIA’s cutting-edge platforms need advanced infrastructure solutions. AI deployments can count on Vertiv’s leadership in power and cooling to keep their AI running no matter the cluster size.

Discover the future of AI with Vertiv and NVIDIA 

Supporting Intel’s latest generation AI accelerator

Vertiv is collaborating with Intel to provide liquid- and air-cooled solutions for the revolutionary Gaudi3 AI accelerator. Our liquid cooled solution has been tested at 160kW accelerator power using facility water from 17°C to 45°C (62.6°F to 113°F). The air-cooled solution has been tested up to 40kW of heat load that can be deployed in warm ambient air data centers up to 35°C (95°F).

Dive into the Vertiv-Intel collaboration

phone-mockup.png

Simulate the air-to-liquid cooling transition in Augmented Reality

 

Make the transition to hybrid and liquid-based cooling for your facility in augmented reality and experience the power of our high-density solutions first-hand, through Vertiv™ XR

SCAN TO START

bologna-career-fair-xr-qr-10.png
oculus_vvs-1.png

Explore High-Density Liquid Cooling Solutions in Virtual Reality

Orchestrate the thermal system upgrade needed, to support your high-density application, then deep-dive into the exploration of the liquid cooling solutions that make it possible in virtual reality, through the Vertiv™ Virtual Showroom.

SCAN TO TRY ON YOUR PHONE

bologna-career-fair-vvs-qr-1.png

Talk to an expert

Please fill out the form below and we will get back to you as soon as possible.

Privacy notice consent

Having received and read this privacy notice on personal data processing (provided in accordance with Article 13 of EU Regulation 679/2016), I consent to:

The processing of my personal data for marketing purposes, including staying informed by email about industry trends, events, offers and product launches.

     Processing request ...
Your submission has been received!
Thank you for reaching out to us.

AI library

Are you ready to start eliminating the heat loads created by your
high-performance compute application?

 

Language & Location