- DCD Broadcast: Is direct to chip cooling leading the pack?
- 2023/05/11 13:00
- 0001/01/01 00:00
- 五月 11, 2023
As GPUs and CPUs continue to densify, they are rapidly surpassing the limits of air cooling. This, coupled with the advent of AI and ML, which is being rolled out on a commercial scale, is accelerating the need for far more efficient types of cooling which can rapidly move heat away from the rack. So, could direct-to-chip be the solution? Join Vertiv and accompanying industry experts in this webcast to find out.
Speaker

Nigel Gore
Sr. Director, Liquid Cooling, Vertiv
Nigel’s experience focuses on IT Infrastructure product and strategy development. His focus is the growing demand for applications like Artificial Intelligence, Scientific Computing and Autonomous Systems which are driving the need for higher density compute architectures requiring advanced cooling solutions. Nigel holds an MBA in digital technology from University of Newcastle in Australia, and he and his family reside in the UK.