Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Alternative Energy to Offer Connectivity in the Paraguayan Chaco

2022年2月24日

Background:

Taking into consideration the absence of power grids in this remote area and its need for sustainability, solar energy was the most viable option to power the mobile radio base station in this area, which has a low population density and no existing telephone service.

Results:

  • Optimized data center cooling
  • Continuous increase in energy efficiency to support sustainability goals
  • Project completion in just nine months during a global pandemic

 

Case Summary
Location:​

Paraguayan Chaco, Paraguay

Critical Need:

The remote area, and its need for sustainability, revealed solar energy was the most viable option to power the mobile radio base station in this area, which has a low population density and no existing telephone service.

Vertiv Solution:
  • Vertiv™ NetSure™ 5100 DC Power System with NetSure™ controller for remote access.
  • Vertiv™ EPC 48300/2900 Outdoor Cabinet with Lithium Ion Batteries
  • NetSure™ S48-2000e3 - Solar Converters
  • NetSure™ Solar Panels and Solar Panel Protection Boxes
  • Support structure for solar panels



DOWNLOAD THE CASE STUDY

Language & Location