Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Thermal Management Solution for Unmanned Pre-fabricated Container

Background

Unmanned pre-fabricated containers (prefab house) are meant to accommodate all the necessary equipment from power source, electrical distribution and active loads in as much as possible optimized space, since any increase in space can potentially lead to Total Cost of Ownership (TCO). Now in such scenario, densely populated enclosed space can be catastrophic and lead to complete system breakdown. Therefore the entire prefab infrastructure needs to be air conditioned to maintain optimum inside environment.

This success story explains - how Vertiv helps prefab houses in overcoming the critical cooling challenges with its Thermal Management expertise and showcases how Vertiv has designed and deployed Precision Cooling solution for remote and scattered located pre-fabricated containers.

Case Summary

Location: Tumkur, South India
Critical Needs:

  • Precision Air Conditioning solution to handle heat load of prefab house made of steel, along with proper thermal insulation
  • Air conditioning system should operate 24 x 7 without standby unit (due to space constraint)
  • Maintain the optimum temperature of 25 °C ±1 °C & relative humidity and 50% ±5% RH
  • Air should properly distribute to confirm zero hot spots within container
  • Speed deployment within eight weeks

Vertiv Solutions:
A Precision Air Conditioning (PAC) solution of 120 kW DX Unit (Liebert® PDX series) + Liebert® HCR series condenser.

DOWNLOAD THE CASE STUDY
PARTNERS
Overview
Consultants Corner
Partner Login

Language & Location