Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Vertiv expands high-density ups family for large-scale AI and critical digital infrastructure in Asia

27/8/26

Vertiv™ PowerUPS 9000 1.8MW model extends the platform introduced earlier this year, delivering scalable, high-power density protection for AI and other mission-critical applications

SINGAPORE [August 24, 2026] – Vertiv (NYSE: VRT), a global leader in critical digital infrastructure, today announced the expansion of its Vertiv™ PowerUPS 9000 uninterruptible power supply (UPS) family with the introduction of the new 1.8 megawatt model. Designed to support large-scale data centers, high-density Artificial Intelligence (AI) environments, and other mission-critical applications, the new system extends the capabilities of the existing Vertiv PowerUPS 9000 platform to 250kw to 1250kw, delivering higher capacity power protection in a compact footprint. The expanded range is now available across Southeast Asia, Australia and New Zealand.

The system incorporates advanced UPS control capabilities developed specifically to address the rapid power swings associated with AI workloads. Battery Shield technology helps reduce unnecessary battery cycling during sudden load transitions, while Input Power Smoothing helps support more predictable input power flow and reduce stress on upstream electrical infrastructure. Together with advanced state-of-charge management, these capabilities help preserve battery availability for backup operations while supporting grid and infrastructure stability in high-density computing environments.

The Vertiv PowerUPS 9000 1.8MW builds on the platform’s high-power density architecture, engineered to help operators manage growing rack densities, constrained white space, and the increasingly dynamic load profiles associated with AI computing environments. The UPS is engineered with a focus on energy efficiency, serviceability, and deployment flexibility and is designed to integrate into broader Vertiv power and thermal infrastructure strategies for high-density AI and enterprise data center applications.

As AI workloads continue to reshape data center operations, power infrastructure is expected to need to adapt to significantly faster and more unpredictable load behavior. Graphics processing unit (GPU) clusters can transition from low utilization to peak demand within milliseconds, creating rapid power fluctuations that can impact batteries, switchgear, generators, transformers, and upstream utility infrastructure. The new 1.8MW model is designed to help operators manage these conditions through high-efficiency power protection, scalable architecture, and advanced controls that support stable operation across highly dynamic load profiles.

“AI is fundamentally changing data center infrastructure requirements across Asia, driving demand for higher-density power systems that can respond faster and manage the effects of these dynamic AI workloads,” said Tony Gaunt, vice president for product management at Vertiv Asia. “With the expansion of the Vertiv™ PowerUPS 9000 family, we are helping customers scale critical power infrastructure to maximum utilization factors while supporting the resilience, flexibility, and operational continuity required for future-ready AI deployments.”

“Traditional UPS systems were not designed for the rapid and repetitive load transitions created by modern GPU environments,” said Arunangshu Chattopadhyay, director of AC power and power distribution at Vertiv Asia. “The latest expansion in the Vertiv PowerUPS 9000 family incorporates Vertiv’s advanced control, patented technologies that help stabilize power behavior during extreme load fluctuations, while preserving battery health and reducing stress on upstream electrical infrastructure.”

Vertiv tested these control technologies using its proprietary AI load simulator across multiple AI workload profiles, battery configurations, duty cycles, and fluctuation ranges. Testing results indicated stable input current behavior despite extreme output variability, suggesting the system can help protect both battery systems and upstream electrical infrastructure under simulated AI operating conditions.

In Singapore, Vertiv has also collaborated with STT Singapore on testing designed to reflect real-world AI infrastructure conditions, including rapid load transitions and the need for tighter coordination between UPS operation, energy storage systems, and upstream power infrastructure.

Additional information about the Vertiv PowerUPS 9000 family and Vertiv’s portfolio of data center power solutions is available at Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-looking statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.


CONTACT
Abigail Kwok
T
+63998 9687825
E Abigail.Kwok@vertiv.com

Related Articles

PORTALS
Overview
Partner Login

Language & Location